Skip Ribbon Commands
Skip to main content
    

Honeywell Metering Software

Many Honeywell meters offer configuration options which are set by using a software tool and an interface. Some meters require setup, for example when used in an M-Bus network.

On this site you find the following information:

  • A table to help you select the right configuration software tool when accessing a meter directly, i.e. when accessing the meter over its integrated optical interface

  • A table to help you select the right configuration software tool for M-Bus and RF network configuration and remote access to meters

Configuration Software for Direct Meter Access

The following table shows software required for configuration directly at the meter. Apart from the software package – which can be downloaded free of charge – a BT optical interface is required (order number EWA3001799) and the PC consequently must have Bluetooth capability

The table is sorted by application and within the application by Series.

How to determine to which Series an OS Number belongs?

The Series is the same as the first four or five numerals or characters of the OS Number. Examples:

  • OS# EW7730M1200 belongs to EW773 Series
  • OS# EW1300BM1200 and EW1301BM1200 both belong to EW130 Series
Item OS-Numbers starting Software
Water Meters    
EW100 Series Singlejet Water Meters EW100 No configuration possible
EW105 Series Singlejet Pulseout Water Meters EW105 No configuration possible
EW110 Series Singlejet Water Meters without communication module EW110 No configuration possible

M-Bus module for EW110 Series

EWA110C...-MBUS EWASET-MBUS

Pulse out module for EW110 Series

EWA110C...-PO EWASET-PO
EW120 Series Multijet Wet Dial Water Meters EW120 No configuration possible
EW130 Series Multijet Water Meters    

F type: RF

EW1300BF, EW1301BF IzarSet

M type: M-Bus

EW1300BM, EW1301BM HydroSet
EW147, EW148 Singlejet Water Meters EW147, EW148 No configuration possible
EW170 Series Bulk Water Meters    

A type: no communication

EW1700AA, EW1701AA No configuration possible

M type: M-Bus

EW1700BM, EW1701BM HydroSet
EW171 Series Woltman Bulk Water Meters without communication module EW171 No configuration possible

M-Bus module for EW171 Series

EWA171C-MBUS EWASET-MBUS

Pulse out module for EW171 Series

EWA171C-PO EWASET-PO
Heat Meters    
EW447-452 Multijet Heat and Chilled Water Meters EW447, EW448, EW449, EW450, EW451, EW452 HydroSet
EW773 Ultrasonic Heat and Chilled Water Meters (2nd generation = type 775) – marked ‘Typ 775’ on frontplate EW773 IzarSet
EW773 Ultrasonic Heat and Chilled Water Meters (1st generation = type 773) – marked ‘Typ 773’ on frontplate EW773 HydroSet
Flow Meters    
EW370 Series Woltman Flow Meters EW370 No configuration possible
EW457 Series Woltman Flow Meters EW457 No configuration possible
EW473 Series Ultrasonic Flow Meters EW473 No configuration possible
Energy Calculators    
EW500 Energy Calculator EW500 EW500SET
EW545 Energy Calculator (2nd generation = type 548) – marked ‘Typ 548’ on frontplate EW545 IzarSet
EW545 Energy Calculator (1st generation = type 545) – marked ‘Typ 545’ on frontplate EW545 HydroSet

Note: with EW773 and EW545 Series 2nd generation and EW500 some functions are protected and require a USB dongle to be accessible. The dongle allows access to the meter in “expert” mode. A configuration table showing which functions can be changed in standard and which can be changed in expert mode is in the download area.

Configuration Software for Network Masters and Remote Meter Access

The following table shows software required for configuration of M-Bus master units and remote configuration of meters. Apart from the software package - which can be downloaded free of charge - further hardware is required:

  • For M-Bus network configuration: a USB cable for connection to M-Bus master units (supplied with master unit but often not stored at device)
  • For mobile RF network configuration: a BT receiver and a PC with Bluetooth capability

The table is sorted by application and within the application by Series.

Item OS-Numbers starting Software
Water Meters    
EW100 Series Singlejet Water Meters EW100 No remote configuration possible
EW147, EW148 Singlejet Water Meters EW147, EW148 No configuration possible
EW130 Series Multijet Water Meters    
F type: with RF communication EW1300BF, EW1301BF IzarPocket
M type: with M-Bus EW1300BM, EW1301BM Depends on M-Bus master – see below
EW170 Series Bulk Water Meters    
A type: no communication EW1700AA, EW1701AA No configuration possible
M type: M-Bus EW1700BM, EW1701BM Depends on M-Bus master – see below
Heat Meters    
EW447-452 Multijet Heat and Chilled Water Meters    
A type: no communication EW447A, EW448A, EW449A, EW450A, EW451A, EW452A No remote configuration possible
F type: with RF communication EW447F, EW450F IzarPocket
M type: with M-Bus EW447M, EW448M, EW449M, EW450M, EW451M, EW452M Depends on M-Bus master – see below
P type: with pulse output EW447P, EW448P, EW449P, EW450P, EW451P, EW452P No remote configuration possible
EW773 Ultrasonic Heat and Chilled Water Meters (2nd generation = type 775) – marked ‘Typ 775’ on frontplate    
A type: no communication module installed EW7730A, EW7731A No remote configuration possible
F type: with RF onboard EW7730F, EW7731F IzarPocket
K type: with factory installed M-Bus and pulse output modules EW7730K, EW7731K Depends on M-Bus master – see below
M type: with factory installed M-Bus module EW7730M, EW7731M Depends on M-Bus master – see below
Any EW773 (type 775) with installed M-Bus module EW773 + EWA3022071 Depends on M-Bus master – see below
EW773 Ultrasonic Heat and Chilled Water Meters (1st generation = type 773) – marked ‘Typ 773’ on frontplate    
A type: no communication module installed EW7730A, EW7731A No remote configuration possible
K type: with factory installed M-Bus and pulse output modules EW7730K, EW7731K Depends on M-Bus master – see below
M type: with factory installed M-Bus module EW7730M, EW7731M Depends on M-Bus master – see below
Any EW773 (type 773) with installed M-Bus module EW773 + EWA54200001 Depends on M-Bus master – see below
Any EW773 (type 773) with installed RF module EW773 + EWA54200017 HydroPocket
Flow Meters    
EW457 Series Woltman Flow Meters EW457 No configuration possible
EW473 Series Ultrasonic Flow Meters EW473 No configuration possible
Energy Calculators    
EW545 Energy Calculator (2nd generation = type 548) – marked ‘Typ 548’ on frontplate    
A type: no communication module installed EW545 No remote configuration possible
Any EW545 (type 548) with installed M-Bus module EW545 + EWA3022071 Depends on M-Bus master – see below
EW545 Energy Calculator (1st generation = type 545) – marked ‘Typ 545’ on frontplate    
A type: no communication module installed EW545 No remote configuration possible
Any EW545 (type 545) with installed M-Bus module EW545 + EWA54200001 Depends on M-Bus master – see below
Any EW545 (type 545) with installed RF module EW545 + EWA54200017 HydroPocket
M-Bus Master Units and System Components    
EW535M0050…0053 HydroCenter M-Bus Master Units   HydroCenter
EW535M0056…0059 HydroPort M-Bus Converters   HydroPort
EW535M0093…0094 HydroCenter 25 M-Bus Master Units   HydroCenter
EW535M0131 M-Bus Receiver   IzarCenter
EW535M5777…5783 IzarCenter M-Bus Master Units   IzarCenter
EW9100AFZ001 External M-Bus Module   IzarPocket